xCarrier Overview
xCarrier Supplier Shipping
Guidelines
xCarrier FAQ
- How many days earlier than the PO
STD can I process shipment?
- How many days later than the PO
STD can I process a shipment?
- What is the difference between
Auto Pack, Pack All, and Pack?
- What do I do if I need to ship an
item from an address that I have not used before?
- What do I need to do to look up a
shipment that I have already processed?
- What is serial number column used
for?
- What if I want to see what lines
are shipped in a shipment?
- What if the Administration tab is
missing from xCarrier?
- What if there are no lines
available to ship but I have an open Qty on a PO?
- What do I do if a part requires
source inspection?
- What if I receive an error
message “missing or invalid shipper numbers”?
xCarrier Support Available
24/7
·
Select link to send a question or issue AEROxCarrierSuport
|